9.15.8.36 Example

The following example sets the VPUMP option to OFF and uses the TCK frequency specified in the programmer file (force_freq is set to OFF).

configure_flashpro3_prg –vpump {OFF} –force_freq {OFF}

configure_flashproLite_prg

Changes Actel FlashPro Lite programmer settings.

configure_flashproLite_prg [-vpp {ON|OFF}] [-vpn {ON|OFF}] [-drive_trst {ON|OFF}] [-force_freq {ON|OFF}] [-freq {freq}]