9.15.8.60 Example

The following example dumps your Tcl commands into the file 'tcldump.tcl'

dump_tcl_support -file {tcldump.tcl}

enable_device

enable_device -name {name} -enable {TRUE|FALSE}

Enables or disables a device in the chain (if the device is disabled, it is bypassed). Chain programming mode must be set. The device must be an Actel device.