9.15.8.40 Example

The following example sets the programmer to drive the VPP, drive VPN, drive the TRST and uses the frequency set by the programmer file (sets force_freq to OFF):

configure_flashprolite_prg –vpp {ON} –vpn {ON} –drive_trst {ON} –force_freq {OFF}

connect_cable

Connects a parallel cable to a port.

connect_cable -cable_name {cable_name} -port_name {port_name} [-drive_trst {ON|OFF}]