10.4.4.5.2 Read Operation
During a read operation when the RE signal is asserted the FIFO reads a data value onto the Q bus from the memory. The data is available to the client 2 clock cycles after the assertion of the RE, this data is held on the bus until the next RE is asserted. The DVLD signal is asserted on the same clock cycle that the data is available. Therefore, the client logic can monitor the DVLD signal for indication of valid data. However, DVLD only asserts for the first clock cycle that the new data is available, whereas the actual data may still be on the data bus.
If the FIFO is emptied then the EMPTY flag is asserted to indicate that no more data elements can be read. The AEMPTY flag is asserted when the number of elements in the FIFO equals the set threshold amount.
If a read operation is attempted while the FIFO is empty, the UNDERFLOW signal is asserted on the next clock cycle indicating that an error has occurred. The UNDERFLOW signal is asserted for each read operation that fails.
A sample timing diagram of a FIFO with depth configuration of 4, almost empty value set to 1, and rising clock edge is shown in the following figure.