21.3.57 import_component
(Ask a Question)Description
This Tcl command imports a component *.cxf
file into the Libero project. After
import, the *.cxf
file is placed in the
<project_folder>/component/work/<component_name>
folder.
Note: Only the
*.cxf
file format is
supported for component import.import_component -file <path_to_component.cxf>
Arguments
Parameter | Type | Description |
---|---|---|
file | string | The -file argument specifies the location of the component *.cxf
file to import. Both absolute and relative paths are
supported. |
Error Codes
Error Code |
Description |
---|---|
None |
Could not find the specified core file. |
None |
Required parameter 'file' is missing. |
None |
Parameter 'param_name' is not defined. |
Supported Families
Supported Families |
---|
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following example imports a component my_mult.cxf file into the Libero project.
import_component -file {D:/test/my_design/my_mult.cxf}