21.3.37 export_fp_pdc
(Ask a Question)Description
This Tcl command exports the Floorplanning Physical Design Constraint (*.pdc) File. You can export the Floorplan PDC file from Constraint Manager > I/O Attributes or Constraint Manager Floor Planner or from File menu. Constraints can be exported to PDC file for reference, but must be manually added to an existing PDC or imported via the Constraints Editor for the changes to affect the final paced and routed design. The exported file has *.pdc file name extension. Before exporting, you need to run 'Place and Route'.
export_fp_pdc \
-file { absolute or relative path and name of *.pdc file } \
[-mode { PDC_PLACE | PDC_FULL_PLACEMENT }]
Arguments
Parameter | Type | Description |
---|---|---|
file | string | Specifies absolute or relative path and name of the *.pdc file. It is mandatory. |
mode | string | Choose the type of information that you want to export. Use PDC_PLACE to export user’s floorplanning constraints, for example, fixed logic and regions. Use |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'file' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'export_fp_pdc -file "Export File Name" [-mode "Export Mode"] '. |
Supported Families
Supported Families |
---|
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following example exports information about all of the physical designs constraints (I/O constraints, I/O Banks, routing constraints, region constraints, global and local clocks).
export_fp_pdc -file {E:/designs/export/sd1_fp.pdc} \
-mode {PDC_FULL_PLACEMENT}