21.3.53 get_libero_release
(Ask a Question)Description
This Tcl command returns the release number of the Libero SoC release. The value that is returned is the same as the release number that is displayed in the
.get_libero_release
Arguments
Return Type | Description |
---|---|
string | Return the release number of the Libero SoC release. |
Supported Families
Supported Families |
---|
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following example displays Libero release number with var1 variable.
get_libero_release
#save into a variable
set var1 [get_libero_release]
#display the variable
puts "Libero Release is $var1"
You will see output similar to the following.
Libero Version is 12.6.0