21.3.16 close_design
(Ask a Question)Description
This Tcl command closes the current design and brings Designer to a fresh state to work on a new design. This is equivalent to selecting the Close command from the File menu.
close_design -component "smartdesign component name"
Arguments
Parameter | Type | Description |
---|---|---|
component | string | Specifies the name of the SmartDesign component to be closed. It is mandatory. |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'component' is missing. |
None | Parameter 'component' has illegal value. |
Supported Families
Supported Families |
---|
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following example checks is the "Top" design component successfully closed or no.
if {[ catch {close_design -component {Top}} ]} {
puts “Failed to close design”
# Handle Failure
} else {
puts “Design closed successfully”
# Proceed with processing a new design
}