21.3.75 remove_profile
(Ask a Question)Description
This Tcl command deletes a tool profile.
remove_profile -name profilename
Arguments
Parameter | Type | Description |
---|---|---|
name | string | Specifies the name of the profile you wish to delete. |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'name' is missing. |
None | Parameter 'name' has illegal value. |
None | Profile 'profilename' does not exist. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'remove_profile -name "profile name"'. |
Supported Families
Supported Families |
---|
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following command deletes the profile 'custom1'.
remove_profile -name "custom1"