21.3.77 rename_library
(Ask a Question)Description
This Tcl command renames a VHDL library from your project. To renames library, right-click the design module name in the Design Hierarchy select Rename VHDL Library from the context menu.
rename_library -library "library name" -name "library new name"
Arguments
Parameter | Type | Description |
---|---|---|
library | string | Identifies the current name of the library that you wish to rename. |
name | string | Specifies the new name of the library. |
Error Codes
Error Code | Description |
---|---|
None | Required parameter 'library' is missing. |
None | Required parameter 'name' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'rename_library -library "old library name" -name "new library name"' . |
Supported Families
Supported Families |
---|
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example renames a library from 'my_lib' to 'my_new_lib'.
rename_library -library "my_lib' -name "my_new_lib"