21.3.47 export_script
(Ask a Question)Description
This Tcl command explicitly exports the Tcl command equivalents of the current Libero session. With this command you can re-execute the same commands interactively or in batch.
You must supply a file name with the -file
parameter and the -relative_path
parameter to specify whether an absolute or relative path is used in the exported script file.
export_script \
-file { absolute or relative path to constraint file } \
-relative_path <value>
Arguments
Parameter | Type | Description |
---|---|---|
file | string | Specifies the absolute or relative path and name to the exported script file. |
relative_path | boolean | Sets your option to use a relative or absolute path in the exported script; use 1 for relative path, 0 for absolute. |
Error Codes
Error Code | Description |
---|---|
None | Parameter 'file' has illegal value. |
None | Required parameter 'relative_path' is missing. |
Supported Families
Supported Families |
---|
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following command exports the Tcl command equivalents of the current Libero session.
export_script -file {./exported.tcl} -relative_path 1