21.3.34 export_component_to_tcl
(Ask a Question)Description
This Tcl command exports the Tcl command for the selected component. The components can be SmartDesign components, configured cores and HDL+ cores.
export_component_to_tcl -component component_name \
[-library "library_name" ] \
[-package "package_name" ] \
[-recursive "TRUE | FALSE"] \
[-folder "folder"] \
[-file "file_path"]
Arguments
Parameter | Type | Description |
---|---|---|
component | string | Specifies the name of the component for which the Tcl command is exported. It is mandatory. |
library | string | Specifies the name of the library the component belongs to. It is optional. |
package | string | Specifies the name of the package the HDL+core belongs to. It is optional. |
recursive | boolean | Specifies if a SmartDesign component needs to be exported recursively. It is optional. |
file | string | Specifies the path where you wish to export the Tcl file. It is mandatory. |
Error Codes
Error Code | Description |
---|---|
None | Please specify a file path for the 'file' parameter. |
None | Required parameter 'component' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'export_component_to_tcl -component "component name" [-library "library name"] [-package "package name"] [-file "file"] [-recursive "TRUE | FALSE"] [-folder "folder"] '. |
Supported Families
Supported Families |
---|
PolarFire® |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following command exports the Tcl command for "work" library "pattern_gen_checker" component.
export_component_to_tcl -component {pattern_gen_checker} \
-library {work} -package {} folder {} \
-file {./pattern_gen_checker.tcl}