21.3.87 set_global_include_file
(Ask a Question)Description
This Tcl command for setting a file as global include file.
set_global_include_file -file {filename}
Arguments
Parameter | Type | Description |
---|---|---|
file | string | The user provides the file path to set as global include file. The file path can be absolute path, linked files path or path with Environment variable from project settings. |
Return Type | Description |
---|---|
None | None |
Error Codes
Error Code | Description |
---|---|
None | Invalid Global Include File 'value'. |
None | Parameter 'file' has illegal value. |
None | Required parameter 'file' is missing. |
None | Parameter 'param_name' is not defined. Valid command formatting is 'set_global_include_file -file "set global include file"'. |
Supported Families
Supported Families |
---|
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
This example sets global include file with absolute file path.
set_global_include_file -file {E:\prj\global_include_files\hdl\add.h}
ENV from Project settings
set_global_include_file -file {${ENV_2}/xyz.h}
Linked Files TCL variable
set_global_include_file -file "$proj/hdl/abcd.v"