This register counts the number of frames that had GRXER asserted
during reception. For 10/100 mode symbol errors are counted regardless of frame
length checks. For Gigabit
mode the frame must satisfy slot time requirements in order to count a symbol
error. Additionally, in Gigabit half duplex mode, carrier extension errors are
also recorded. Receive symbol errors will also be counted as an FCS or
alignment error if the frame is between 64 and 1518 bytes (1536 bytes if bit 8 is set
in the Network Configuration Register, 10240
bytes if bit 3 is set in the Network Configuration Register). If the frame is
larger it will be recorded as a jabber error. See GMAC Network Configuration
Register.