3.3.26.4 mcPosI_PositionControlAuto
C
/* Perform automatic position control */
void mcPosI_PositionControlAuto( const tmcPos_Parameters_s * const pParameters,
const float32_t ref, const float32_t act, float32_t * const pOut )
Summary
Perform the position control operation.
Description
This function controls rotor position using a PI controller. It calculates the error between the reference and actual position, controls the position error using the PI controller based on the state of the position control module, and updates the reference speed value.
Precondition
The position control module must be initialized and enabled.
Parameters
| Param | Description |
|---|---|
| pParameters | A pointer to the position control module parameter structure |
| ref | Reference position value. |
| act | Actual position value. |
| pOut | A pointer to a variable where the output of the PI controller will be stored. |
Returns
None
Example
// Define the position control module data structure tmcPos_Parameters_s posParameters; float32_t ref = 1000.0f; float32_t act = 950.0f; float32_t nref /** Execute position control loop */ void mcPosI_PositionControlAuto(&posParameters, ref, act, &nref);
Remarks
None.