4.2.6 Error Response
The error response, which is indicated by the HRESP signal, is asserted if any of the following conditions occur:
- AHBL burst read is terminated early or address sequence is not as expected. This should never occur within the system during normal operation.
- AHBL write transaction addressed to read-only user data array
- AHBL read or write transaction to a protected memory area. Refer to Security.
Data on HRDATA with error response is zero. A write transaction addressed to read-only Control register such as RD or RDT will not trigger an error response. However, the data in these registers will not be affected.