2.6.3.4.2 LSR
Logical shift right by n bits moves the left-hand 32-n bits
of the register Rm, to the right by n places, into the right-hand
32-n bits of the result. And it sets the left-hand n bits of the result to 0. See
the following figure.
You can use the LSR #n operation to divide the value in
the register Rm by 2n, if the value is
regarded as an unsigned integer.
When the instruction is LSRS or when LSR
#n is used in Operand2 with the instructions
MOVS, MVNS, ANDS,
ORRS, ORNS, EORS,
BICS, TEQ or TST, the carry flag is
updated to the last bit shifted out, bit[n-1], of the register Rm.
- If n is 32 or more, then all the bits in the result are cleared to 0.
- If n is 33 or more and the carry flag is updated, it is updated to 0.