2.6.10.11.2 Operation
WFE is a hint instruction.
If the event register is 0, WFE suspends execution until one of the following events occurs:
an exception, unless masked by the exception mask registers or the current priority level
an exception enters the Pending state, if SEVONPEND in the System Control Register is set
a Debug Entry request, if Debug is enabled
an event signaled by a peripheral or another processor in a multiprocessor system using the SEV instruction.
If the event register is 1, WFE clears it to 0 and returns immediately.
For more information see Power Management.
Condition flags
This instruction does not change the flags.
Examples
WFE ; Wait for event