9.3 How to Use USB OTG Controller
Microchip recommends the following flow for configuring the USB OTG controller.
- Instantiate the SmartFusion 2 MSS component into the Libero SoC project
- Configure (enable/disable) the SmartFusion 2 MSS components as per the application needs using the MSS configurator
- Configure the USB OTG controller as explained in the following sections
Important: The MSS USB does not support full behavioral
simulation models. For more information, see SmartFusion2 MSS BFM Simulation User Guide.