2.110.81 SERCOMx_I2C_TransferDirGet Function
C
/* x = SERCOM instance number */
/* I2C slave mode */
SERCOM_I2C_SLAVE_TRANSFER_DIR SERCOMx_I2C_TransferDirGet(void)
Summary
Returns the I2C transfer direction
Description
This function returns the I2C transfer direction
Precondition
SERCOMx_I2C_Initialize must have been called for the associated SERCOM I2C instance
Parameters
None.
Returns
SERCOM_I2C_SLAVE_TRANSFER_DIR_WRITE - I2C master is writing data to I2C slave
SERCOM_I2C_SLAVE_TRANSFER_DIR_READ - I2C master is reading data from I2C slave
Example
The below code snippet shows the use of the SERCOMx_I2C_TransferDirGet() API when SERCOM I2C slave PLIB is used in polled mode (interrupt is disabled).
static bool isFirstByteSent;
static bool transferDir;
SERCOM_I2C_SLAVE_INTFLAG intFlags = SERCOM0_I2C_InterruptFlagsGet();
if (intFlags & SERCOM_I2C_SLAVE_INTFLAG_AMATCH)
{
isFirstByteSent = false;
// Read and save the transfer direction in a global variable.
transferDir = SERCOM0_I2C_TransferDirGet();
// Send ACK succeeded by reception of next byte
SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_SEND_ACK);
}
else if (intFlags & SERCOM_I2C_SLAVE_INTFLAG_DRDY)
{
if (transferDir == SERCOM_I2C_SLAVE_TRANSFER_DIR_WRITE)
{
// I2C master is writing data to I2C slave. Read the received byte.
rxByte = SERCOM0_I2C_ReadByte();
// Execute acknowledge action succeeded by reception of next byte
SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_SEND_ACK);
}
else
{
// I2C master is reading data from I2C slave. Check if the previous data
// is acknowledged by the I2C master.
if (isFirstByteSent == false)
{
SERCOM0_I2C_WriteByte(txData);
isFirstByteSent = true;
}
else
{
if (SERCOM0_I2C_LastByteAckStatusGet() == SERCOM_I2C_SLAVE_ACK_STATUS_RECEIVED_ACK)
{
// Last byte was acknowledged by the I2C master; send another byte.
SERCOM0_I2C_WriteByte(txData);
//Execute a byte read operation followed by ACK/NACK reception
SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_RECEIVE_ACK_NAK);
}
else
{
// Last byte was NAK'd by the I2C master; wait for start condition.
//Wait for any start (S/Sr) condition
SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_WAIT_FOR_START);
}
}
}
}
Remarks
None.