2.110.84 SERCOMx_I2C_CommandSet Function
C
/* x = SERCOM instance number */
/* I2C slave mode */
void SERCOMx_I2C_CommandSet(SERCOM_I2C_SLAVE_COMMAND command)
Summary
Sets I2C slave command
Description
Sets I2C slave command. The I2C slave state machine takes action based on the set command.
Precondition
SERCOMx_I2C_Initialize must have been called for the associated SERCOM I2C instance
Parameters
| Param | Description |
|---|---|
| SERCOM_I2C_SLAVE_COMMAND_SEND_ACK | Send ACK succeeded by reception of next byte |
| SERCOM_I2C_SLAVE_COMMAND_SEND_NAK | Send NAK succeeded by reception of next byte |
| SERCOM_I2C_SLAVE_COMMAND_RECEIVE_ACK_NAK | Execute a byte read operation followed by ACK/NACK reception |
| SERCOM_I2C_SLAVE_COMMAND_WAIT_FOR_START | Wait for any start (S/Sr) condition |
Returns
None.
Example
The below code snippet shows how SERCOMx_I2C_CommandSet() API can be used when SERCOM I2C slave PLIB is used in polled mode (interrupt is disabled).
static bool isFirstByteSent;
static bool transferDir;
// Define a flag that inidicates if the I2C slave application is busy or ready
static bool isAppBusy;
SERCOM_I2C_SLAVE_INTFLAG intFlags = SERCOM5_I2C_InterruptFlagsGet();
if (intFlags & SERCOM_I2C_SLAVE_INTFLAG_AMATCH)
{
isFirstByteSent = false;
// Read and save the transfer direction in a global variable.
transferDir = SERCOM5_I2C_TransferDirGet();
if (isAppBusy == true)
{
// I2C slave application is busy. Send NAK.
SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_SEND_NAK);
}
else
{
// I2C slave application is ready. Send ACK succeeded by reception of next byte
SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_SEND_ACK);
}
}
else if (intFlags & SERCOM_I2C_SLAVE_INTFLAG_DRDY)
{
if (transferDir == SERCOM_I2C_SLAVE_TRANSFER_DIR_WRITE)
{
// I2C master is writing data to I2C slave. Read the received byte.
rxByte = SERCOM0_I2C_ReadByte();
// Execute acknowledge action succeeded by reception of next byte
SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_SEND_ACK);
}
else
{
// I2C master is reading data from I2C slave. Check if the previous data
// is acknowledged by the I2C master.
if (isFirstByteSent == false)
{
SERCOM0_I2C_WriteByte(txData);
isFirstByteSent = true;
}
else
{
if (SERCOM0_I2C_LastByteAckStatusGet() == SERCOM_I2C_SLAVE_ACK_STATUS_RECEIVED_ACK)
{
// Last byte was acknowledged by the I2C master; send another byte.
SERCOM0_I2C_WriteByte(txData);
//Execute a byte read operation followed by ACK/NACK reception
SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_RECEIVE_ACK_NAK);
}
else
{
// Last byte was NAK'd by the I2C master; wait for start condition.
//Wait for any start (S/Sr) condition
SERCOM0_I2C_SendCommand(SERCOM_I2C_SLAVE_COMMAND_WAIT_FOR_START);
}
}
}
}
else if (intFlags & SERCOM_I2C_SLAVE_INTFLAG_PREC)
{
SERCOM0_I2C_InterruptFlagsClear(SERCOM_I2C_SLAVE_INTFLAG_PREC);
}
Remarks
This API is generated when Smart mode is disabled and is typically used when the SERCOM I2C slave PLIB is used in polled mode (interrupt is disabled).