2.110.27 SERCOMx_USART_LIN_CommandSet Function
C
/* x = SERCOM instance number */
/* Blocking, non-blocking and ring buffer mode */
bool SERCOMx_USART_LIN_CommandSet(USART_LIN_MASTER_CMD cmd)
Summary
This API lets the application to select between automatic transmission of the complete LIN header or software controlled transmission of LIN header in LIN master mode.
Description
This API lets the application to select between automatic transmission of the complete LIN header or software controlled transmission where various header components are controlled by software. The LIN header consists of break character followed by a Sync byte followed by a PID byte. This API is only available when LIN Master mode is selected in MCC.
Precondition
SERCOMx_USART_Initialize must have been called for the associated SERCOM_USART instance.
Parameters
| Param | Description |
|---|---|
| USART_LIN_MASTER_CMD_SOFTWARE_CONTROLLED | LIN header frame is controlled by software |
| USART_LIN_MASTER_CMD_AUTO_TRANSMIT | LIN header frame is transmitted automatically byhardware |
Returns
true - operation is successful
false - operation is unsuccessful. LIN command strobe must not be issued when the transmitter is busy.
Example
if (SERCOM0_USART_LIN_CommandSet(USART_LIN_MASTER_CMD_AUTO_TRANSMIT) == true)
{
txBuffer[0] = 0x80; // PID value
// Transmit the LIN frame (Break + Sync + PID)
SERCOM0_USART_Write(txBuffer, 1);
}
Remarks
This API is only available on the devices that has LIN support.