2.110.28 SERCOMx_ISO7816_Card_Detect
C
/* x = SERCOM instance number */
bool SERCOMx_ISO7816_Card_Detect( void )
Summary
This API provides the physical card available status.
Description
This API allows the application to detect the physical card available status. The gpio pin configured as input reads high if the card if the card is present in slot else low. The api returns true if the pin is read high and false if the pin is read low.
Precondition
None
Parameters
None
Returns
True - card is detected
False - card not detected
Example
/* Wait while card detect pin is set */
while( SERCOM3_ISO7816_Card_Detect() != true )
{
/* Do Nothing */
}
Remarks
None