21.12.23.2.1 Bottleneck Options

  • Cost Type: Select the cost type that SmartTime will include in the bottleneck report. By default, path count is selected.
  • Limit the number of reported paths per section to: Specify the maximum number of paths per set type that SmartTime will include per section in the report. The default maximum number of paths reported is 100.
  • Limit the number of parallel paths in expanded path to: For each expanded path, specify the maximum number of parallel paths that SmartTime will include in the report. Only cells that lie on these violating paths are reported. The default number of parallel paths is 1.
  • Limit the number of reported instances: Specify the maximum number of cells that SmartTime will include per section in the report. The default number of cells is 10.