2.1.18.2 Current Monitor and Differential Monitor
For both peripherals, the calculated threshold is determined using the following equation:
Calculated Threshold = User Threshold (A) * Resistor Value (Ω) * Gain * LSB
Value
where:
- User Threshold (A): Is the current threshold specified by the user.
- Resistor Value (Ω): Is the external resistor value specified for the Current Monitor.
- Gain: Is the amplification applied by the Current Monitor and Differential Voltage Monitor (Gain = 10).
- LSB Value: Is the value of one least significant bit, calculated as VREF / 2¹².