2.1.18.1 Voltage Monitor

For the Voltage Monitor, the calculated threshold is determined using the following equation:

Calculated Threshold = User Threshold (V) * Scaling Factor * LSB Value

where:

  • User Threshold (V): Is the voltage threshold specified by the user.
  • Scaling Factor: Is determined by the selected prescaler range.
  • LSB Value: Is the value of one least significant bit, calculated as VREF / 2¹².