1.2.23.5 Real Time Counter (RTC) Clock
The RTC Clock is the clock frequency for the Real Time Counter logic on the chip. This is modeled inside the AB library macro.
The RTC Clock is exposed on the ASB if the RTC peripheral is configured within the tool, that is, not configured externally. Connect this port to the CLKOUT of the XTLOSC macro if in use, otherwise it must be grounded.
This clock has no relationship with any of the other clocks listed here.