FPU WAW Hazards
The WAW (Write-After-Write) hazard is a further consequence of allowing instructions to continue execution while others are stalled or taking longer to execute. As is the case for WAR hazards, instruction writes can end up out of order, leaving an incorrect (stale) value in a destination register.
WAW output dependency is possible because once the coprocessor instruction is issued, the CPU and coprocessor pipelines operate independently. A multi-cycle coprocessor instruction may therefore complete after one or more CPU instructions that were subsequently issued (i.e., out of order). A WAW hazard will exist when the CPU instruction is ready to retire before the coprocessor instruction retires and either:
- The same register is a
destination for both the coprocessor instruction and the CPU instruction that
follows it.
or
- The CPU instruction write targets a coprocessor register that is being used by the prior coprocessor instruction.
In both cases, the resource cannot be shared.
An internal WAW hazard can arise between successive FPU instructions that have differing execution times. However, each issued instruction is tracked by pushing its associated functional unit ID into a FIFO, which is emptied in the same order as it is filled when instructions move results from their functional units into the WB-stage. Should an expected (from the FIFO) functional unit result not be ready, this knowledge is used in the Write stage to complete the destination write in the correct sequence, stalling those instructions that arrive out of order, thereby eliminating the WAW hazard.
If the CPU and FPU pipelines are viewed as conjoined, a WAW hazard is also possible should the CPU attempt to write a value to the same register as also targeted by a previously issued FPU instruction whose write has not yet completed. However, access to the write target(s) of an instruction is inhibited as soon as the instruction is committed (see FPU and CPU Exceptions). Consequently, any attempt by the CPU to write to an FPU register that is already bound to a prior FPU instruction being executed will result in the write grant failure (and the CPU write stalling).
FMOVC
and FMOV
(these ops do not update the FSR),
and FAND and FIOR, unless they will modify the FSR. The FEAR is bound to all FPU
instructions except for FMOVC
, FMOV
and
FTST
. It is also not bound to FAND or FIOR unless it will be
modified by them. Note that this applies irrespective of whether FEAR is enabled or not
(i.e., FEAR.EACE is a “don’t care” with respect to FEAR hazard detection).