1.2.7.4.11 SYS_FS_FileTell Function
1.2.7.4.11 C
int32_t SYS_FS_FileTell
(
SYS_FS_HANDLE handle
);
1.2.7.4.11 Summary
Obtains the file pointer position.
1.2.7.4.11 Description
Obtains the current value of the file position indicator for the file pointed to by handle.
1.2.7.4.11 Precondition
A valid file handle must be obtained before performing a file tell.
1.2.7.4.11 Parameters
| Parameters | Description |
|---|---|
| handle | File handle obtained during file Open |
1.2.7.4.11 Returns
On success - returns the current file position.
On failure - returns -1. The reason for the failure can be retrieved with SYS_FS_Error or SYS_FS_FileError.
1.2.7.4.11 Example
SYS_FS_HANDLE fileHandle; int32_t tell; fileHandle = SYS_FS_FileOpen("/mnt/myDrive/FILE.JPG", (SYS_FS_FILE_OPEN_READ)); if(fileHandle != SYS_FS_HANDLE_INVALID) { // File open is successful } ... ... tell = SYS_FS_FileTell(fileHandle); if(tell != -1) { // Success }
1.2.7.4.11 Remarks
None.