1.2.7.4.24 SYS_FS_FileTestError Function

1.2.7.4.24 C

bool SYS_FS_FileTestError
(
    SYS_FS_HANDLE handle
);

1.2.7.4.24 Summary

Checks for errors in the file.

1.2.7.4.24 Description

This function checks whether or not file has any errors.

1.2.7.4.24 Precondition

A valid file handle must be obtained before passing to the function.

1.2.7.4.24 Parameters

ParametersDescription
handleFile handle obtained during file Open

1.2.7.4.24 Returns

On success returns false indicating that the file has no errors. On failure returns true. The reason for the failure can be retrieved with SYS_FS_Error or SYS_FS_FileError.

1.2.7.4.24 Example

SYS_FS_HANDLE fileHandle;
bool err;

fileHandle = SYS_FS_FileOpen("/mnt/myDrive/FILE.JPG", (SYS_FS_FILE_OPEN_READ));

if(fileHandle != SYS_FS_HANDLE_INVALID)
{
    // File open is successful
}
...
...

err = SYS_FS_FileTestError(fileHandle);

if(err == true)
{
    // either file has error, or there
    // was an error in working with the "SYS_FS_FileTestError" function
}

1.2.7.4.24 Remarks

None.