1.2.7.4.64 SYS_FS_MEDIA_MANAGER_Read Function

1.2.7.4.64 C

SYS_FS_MEDIA_BLOCK_COMMAND_HANDLE SYS_FS_MEDIA_MANAGER_Read
(
    uint16_t diskNo,
    uint8_t* destination,
    uint8_t * source,
    const unsigned int nBytes
);

1.2.7.4.64 Summary

Gets data from a specific media address.

1.2.7.4.64 Description

This function gets data from a specific address of media. This function is intended to work with NVM media only, which can have byte level addressing. For other media, such as a SD card, byte addressing is not possible and this function will not work. Also, this function is intended to work with the MPFS2 file system only, which uses byte addressing.

1.2.7.4.64 Precondition

None.

1.2.7.4.64 Parameters

ParametersDescription
diskNoMedia number
destinationPointer to buffer where data to be placed after read
sourcePointer from where data to be read
nBytesNumber of bytes to be read

1.2.7.4.64 Returns

Buffer handle of type SYS_FS_MEDIA_BLOCK_COMMAND_HANDLE.