1.2.7.4.22 SYS_FS_FileCharacterPut Function

1.2.7.4.22 C

SYS_FS_RESULT SYS_FS_FileCharacterPut
(
    SYS_FS_HANDLE handle,
    char data
);

1.2.7.4.22 Summary

Writes a character to a file.

1.2.7.4.22 Description

This function writes a character to a file.

1.2.7.4.22 Precondition

The file into which a character has to be written, has to be present and should have been opened.

1.2.7.4.22 Parameters

ParametersDescription
handleFile handle to which the character is to be written
dataCharacter to be written to the file

1.2.7.4.22 Returns

SYS_FS_RES_SUCCESS - Write operation was successful.

SYS_FS_RES_FAILURE - Write operation was unsuccessful. The reason for the failure can be retrieved with SYS_FS_Error or SYS_FS_FileError.

1.2.7.4.22 Example

SYS_FS_RESULT res;
SYS_FS_HANDLE fileHandle;

fileHandle = SYS_FS_FileOpen("/mnt/myDrive/FILE.txt", (SYS_FS_FILE_OPEN_WRITE_PLUS));

if(fileHandle != SYS_FS_HANDLE_INVALID)
{
    // File open is successful
}

// Write a character to the file.
res = SYS_FS_FileCharacterPut(fileHandle, 'c');

if(res != SYS_FS_RES_SUCCESS)
{
    // Character write operation failed.
}

1.2.7.4.22 Remarks

None.