1.2.7.4.32 SYS_FS_CurrentWorkingDirectoryGet Function

1.2.7.4.32 C

SYS_FS_RESULT SYS_FS_CurrentWorkingDirectoryGet
(
    char *buff,
    uint32_t len
);

1.2.7.4.32 Summary

Gets the current working directory.

1.2.7.4.32 Description

This function gets the current working directory path along with the working drive.

1.2.7.4.32 Precondition

At least one disk must be mounted.

1.2.7.4.32 Parameters

ParametersDescription
buffPointer to a buffer which will contain the name of the current working directory and drive, once the function completes
lenSize of the buffer

1.2.7.4.32 Returns

SYS_FS_RES_SUCCESS - Get current working directory operation was successful.

SYS_FS_RES_FAILURE - Get current working directory operation was unsuccessful. The reason for the failure can be retrieved with SYS_FS_Error.

1.2.7.4.32 Example

SYS_FS_RESULT res;
char buffer[16];

switch(appState)
{
    case TRY_MOUNT:
    {
        if(SYS_FS_Mount("/dev/mmcblka1", "/mnt/myDrive", FAT, 0, NULL) != SYS_FS_RES_SUCCESS)
        {
            // Failure, try mounting again
        }
        else
        {
            // Mount was successful. Create a directory.
            appState = CREATE_DIR;
        }
        break;
    }

    case CREATE_DIR:
    {
        res = SYS_FS_DirectoryMake("Dir1");
        if(res == SYS_FS_RES_FAILURE)
        {
            // Directory creation failed
            appState = ERROR;
        }
        else
        {
            // Directory creation was successful. Change to the new
            // directory.
            appState = CHANGE_DIR;
        }
        break;
    }

    case CHANGE_DIR:
    {
        res = SYS_FS_DirectoryChange("Dir1");
        if(res == SYS_FS_RES_FAILURE)
        {
            // Directory change failed
            appState = ERROR;
        }
        else
        {
            // Directory change was successful. Get current working
            // directory
            appState = GET_CWD;
        }
        break;
    }

    case GET_CWD:
    {
        res = SYS_FS_CurrentWorkingDirectoryGet(buffer, 15);
        if(res == SYS_FS_RES_FAILURE)
        {
            // Get current directory operation failed
            appState = ERROR;
        }
        break;
    }
}

1.2.7.4.32 Remarks

None.