1.2.7.4 Library Interface
File System Service library provides the following interfaces.
SYS FS Functions
These APIs should be used from application layer to perform any file operation.
| Name | Description |
|---|---|
| SYS_FS_Initialize | Initializes the File System abstraction layer (sys_fs layer) |
| SYS_FS_Tasks | Maintains the File System tasks and functionalities |
| SYS_FS_Mount | Mounts the disk/volume with specified File System |
| SYS_FS_Unmount | Unmounts the disk/volume for the File System |
| SYS_FS_EventHandlerSet | Sets the pointer to the function (and it is context) to be called when mount/unmount event has occurred |
| SYS_FS_FileOpen | Opens a file |
| SYS_FS_FileClose | Closes a file |
| SYS_FS_FileRead | Read data from the file |
| SYS_FS_FileStat | Gets file status |
| SYS_FS_FileSeek | Moves the file pointer by the requested offset |
| SYS_FS_FileTell | Obtains the file pointer position |
| SYS_FS_FileSize | Returns the size of the file in bytes |
| SYS_FS_FileEOF | Checks for end of file |
| SYS_FS_FileNameGet | Reads the file name |
| SYS_FS_Error | Returns the last error |
| SYS_FS_FileError | Returns the file specific error |
| SYS_FS_FileStringGet | Reads a string from the file into a buffer |
| SYS_FS_FileStringPut | Writes a string to a file |
| SYS_FS_FileWrite | Writes data to the file |
| SYS_FS_FileSync | Flushes the cached information when writing to a file |
| SYS_FS_FileTruncate | Truncates a file |
| SYS_FS_FileCharacterPut | Writes a character to a file |
| SYS_FS_FilePrintf | Writes a formatted string into a file |
| SYS_FS_FileTestError | Checks for errors in the file |
| SYS_FS_DirOpen | Open a directory |
| SYS_FS_DirClose | Closes an opened directory |
| SYS_FS_DirRead | Reads the files and directories of the specified directory |
| SYS_FS_DirRewind | Rewinds to the beginning of the directory |
| SYS_FS_DirSearch | Searches for a file or directory |
| SYS_FS_DirectoryMake | Creates a directory |
| SYS_FS_DirectoryChange | Changes to a the directory specified |
| SYS_FS_CurrentWorkingDirectoryGet | Gets the current working directory |
| SYS_FS_FileDirectoryRemove | Removes a file or directory |
| SYS_FS_FileDirectoryRenameMove | Renames or moves a file or directory |
| SYS_FS_FileDirectoryModeSet | Sets the mode for the file or directory |
| SYS_FS_FileDirectoryTimeSet | Sets or changes the time for a file or directory |
| SYS_FS_CurrentDriveGet | Gets the current drive |
| SYS_FS_CurrentDriveSet | Sets the drive |
| SYS_FS_DriveLabelGet | Gets the drive label |
| SYS_FS_DriveLabelSet | Sets the drive label |
| SYS_FS_DriveFormat | Formats a drive |
| SYS_FS_DrivePartition | Partitions a physical drive (media) |
| SYS_FS_DriveSectorGet | Obtains total number of sectors and number of free sectors for the specified drive |
SYS FS Data Types and Constants
| Name | Type | Description |
|---|---|---|
| SYS_FS_HANDLE | Typedef | This type defines the file handle |
| SYS_FS_HANDLE_INVALID | Macro | Invalid file handle |
| SYS_FS_FILE_SYSTEM_TYPE | Enum | Enumerated data type identifying native file systems supported |
| SYS_FS_FILE_DIR_ATTR | Enum | Enumerated data type identifying the various attributes for file/directory |
| SYS_FS_FILE_SEEK_CONTROL | Enum | Lists the various modes of file seek |
| SYS_FS_RESULT | Enum | Lists the various results of a file operation |
| SYS_FS_FORMAT | Macros | Specifies the partitioning rule |
| SYS_FS_FORMAT_PARAM | Struct | SYS FS Drive Format parameter structure |
| SYS_FS_FILE_OPEN_ATTRIBUTES | Enum | Lists the various attributes (modes) in which a file can be opened |
| SYS_FS_ERROR | Enum | Lists the various error cases |
| SYS_FS_EVENT | Enum | Identifies the possible file system events |
| SYS_FS_FUNCTIONS | Struct | SYS FS Function signature structure for native file systems |
| SYS_FS_REGISTRATION_TABLE | Struct | The initialization members for File System layer |
| SYS_FS_FSTAT | Struct | File System status |
| SYS_FS_TIME | Union | The Union to specify the time for a file or directory |
| SYS_FS_EVENT_HANDLER | Typedef | Pointer to the File System Handler function |
SYS FS Media Manager Functions
These APIs should not be directly used from application layer. These can be used internally by media drivers and other clients within Harmony framework if needed.
| Name | Description |
|---|---|
| SYS_FS_MEDIA_MANAGER_AddressGet | Gets the starting media address based on a disk number |
| SYS_FS_MEDIA_MANAGER_CommandStatusGet | Gets the command status |
| SYS_FS_MEDIA_MANAGER_Register | Function to register media drivers with the media manager |
| SYS_FS_MEDIA_MANAGER_DeRegister | Function to De-register media drivers with the media manager |
| SYS_FS_MEDIA_MANAGER_Read | Gets data from a specific media address |
| SYS_FS_MEDIA_MANAGER_SectorRead | Reads a specified media sector |
| SYS_FS_MEDIA_MANAGER_SectorWrite | Writes a sector to the specified media |
| SYS_FS_MEDIA_MANAGER_VolumePropertyGet | Gets the volume property |
| SYS_FS_MEDIA_MANAGER_MediaStatusGet | Gets the media status |
| SYS_FS_MEDIA_MANAGER_EventHandlerSet | Register the event handler for Mount/Un-Mount events |
| SYS_FS_MEDIA_MANAGER_RegisterTransferHandler | Register the event handler for data transfer events |
| SYS_FS_MEDIA_MANAGER_GetMediaGeometry | Gets the media geometry information |
| SYS_FS_MEDIA_MANAGER_TransferTask | Media manager transfer task function |
| SYS_FS_MEDIA_MANAGER_Tasks | Media manager task function |
SYS FS Media Manager Data Types and Constants
| Name | Type | Description |
|---|---|---|
| SYS_FS_MEDIA_BLOCK_COMMAND_HANDLE | Typedef | Handle identifying block commands of the media |
| SYS_FS_MEDIA_BLOCK_COMMAND_HANDLE_INVALID | Macro | Defines the invalid media block command handle |
| SYS_FS_MEDIA_HANDLE | Typedef | Handle identifying the media registered with the media manager |
| SYS_FS_MEDIA_HANDLE_INVALID | Macro | Defines the invalid media handle |
| SYS_FS_MEDIA_BLOCK_EVENT | Enum | Identifies the possible events that can result from a request |
| SYS_FS_MEDIA_PROPERTY | Enum | Contains information of property of a media |
| SYS_FS_MEDIA_STATUS | Enum | The status of media |
| SYS_FS_MEDIA_STATE | Enum | The enumeration for state of media |
| SYS_FS_MEDIA_TYPE | Enum | The enumeration for type of media |
| SYS_FS_MEDIA_COMMAND_STATUS | Enum | The enumeration for status of buffer |
| SYS_FS_MEDIA_REGION_GEOMETRY | Typedef | Contains information of a sys media region |
| SYS_FS_MEDIA_GEOMETRY | Typedef | Contains all the geometrical information of a media device |
| SYS_FS_MEDIA_MOUNT_DATA | Struct | Structure to obtain the device and mount name of media |
| SYS_FS_VOLUME_PROPERTY | Struct | Structure to obtain the property of volume |
| SYS_FS_MEDIA_FUNCTIONS | Struct | Structure of function pointers for media driver |
| SYS_FS_MEDIA_EVENT_HANDLER | Typedef | Pointer to the Media Event Handler function |