1.2.7.4.28 SYS_FS_DirRewind Function
1.2.7.4.28 C
SYS_FS_RESULT SYS_FS_DirRewind
(
SYS_FS_HANDLE handle
);
1.2.7.4.28 Summary
Rewinds to the beginning of the directory.
1.2.7.4.28 Description
This function rewinds the directory to the start. Once a search of directory or directory read is completed, the rewind function is used to begin searching the directory from the start.
1.2.7.4.28 Precondition
A valid directory handle must be obtained before reading a directory.
1.2.7.4.28 Parameters
| Parameters | Description |
|---|---|
| handle | Directory handle obtained during directory open |
1.2.7.4.28 Returns
SYS_FS_RES_SUCCESS - Directory rewind operation was successful.
SYS_FS_RES_FAILURE - Directory rewind operation was unsuccessful. The reason for the failure can be retrieved with SYS_FS_Error or SYS_FS_FileError.
1.2.7.4.28 Example
SYS_FS_HANDLE dirHandle;
SYS_FS_FSTAT stat;
dirHandle = SYS_FS_DirOpen("/mnt/myDrive/Dir1");
if(dirHandle != SYS_FS_HANDLE_INVALID)
{
// Directory open is successful
}
if(SYS_FS_DirRead(dirHandle, &stat) == SYS_FS_RES_FAILURE)
{
// Directory read operation failed.
}
// Do more search
// Do some more search
// Now, rewind the directory to begin search from start
if(SYS_FS_DirRewind(dirHandle) == SYS_FS_RES_FAILURE)
{
// Directory rewind failed.
}
1.2.7.4.28 Remarks
None.