1.2.7.4.53 SYS_FS_ERROR Enum
1.2.7.4.53 C
typedef enum
{
/* Success */
SYS_FS_ERROR_OK = 0,
/* (1) A hard error occurred in the low level disk I/O layer */
SYS_FS_ERROR_DISK_ERR,
/* (2) Assertion failed */
SYS_FS_ERROR_INT_ERR,
/* (3) The physical drive cannot work */
SYS_FS_ERROR_NOT_READY,
/* (4) Could not find the file */
SYS_FS_ERROR_NO_FILE,
/* (5) Could not find the path */
SYS_FS_ERROR_NO_PATH,
/* (6) The path name format is invalid */
SYS_FS_ERROR_INVALID_NAME,
/* (7) Access denied due to prohibited access or directory full */
SYS_FS_ERROR_DENIED,
/* (8) Access denied due to prohibited access */
SYS_FS_ERROR_EXIST,
/* (9) The file/directory object is invalid */
SYS_FS_ERROR_INVALID_OBJECT,
/* (10) The physical drive is write protected */
SYS_FS_ERROR_WRITE_PROTECTED,
/* (11) The logical drive number is invalid */
SYS_FS_ERROR_INVALID_DRIVE,
/* (12) The volume has no work area */
SYS_FS_ERROR_NOT_ENABLED,
/* (13) There is no valid volume */
SYS_FS_ERROR_NO_FILESYSTEM,
/* (14) The Format() aborted due to any parameter error */
SYS_FS_ERROR_FORMAT_ABORTED,
/* (15) Could not get a grant to access the volume within defined period */
SYS_FS_ERROR_TIMEOUT,
/* (16) The operation is rejected according to the file sharing policy */
SYS_FS_ERROR_LOCKED,
/* (17) LFN working buffer could not be allocated */
SYS_FS_ERROR_NOT_ENOUGH_CORE,
/* (18) Number of open files */
SYS_FS_ERROR_TOO_MANY_OPEN_FILES,
/* (19) Given parameter is invalid */
SYS_FS_ERROR_INVALID_PARAMETER,
/* (20) Too many mounts requested. Not enough free volume available */
SYS_FS_ERROR_NOT_ENOUGH_FREE_VOLUME,
/* (21) Requested native file system is not supported */
SYS_FS_ERROR_FS_NOT_SUPPORTED,
/* (22) Requested native file system does not match the format of volume */
SYS_FS_ERROR_FS_NOT_MATCH_WITH_VOLUME,
/* (23) Function not supported in native file system layer */
SYS_FS_ERROR_NOT_SUPPORTED_IN_NATIVE_FS,
/* Below enumerations constants are generated for littleFS only */
/* (24) Error during device operation*/
SYS_FS_ERROR_IO,
/* (25) Corrupted*/
SYS_FS_ERROR_CORRUPT,
/* (26) No directory entry*/
SYS_FS_ERROR_NOENT,
/* (27) Entry already exists*/
SYS_FS_ERROR_ALREADY_EXIST,
/* (28) Entry is not a dir*/
SYS_FS_ERROR_NOTDIR,
/* (29) Entry is a dir*/
SYS_FS_ERROR_ISDIR,
/* (30) Dir is not empty*/
SYS_FS_ERROR_NOTEMPTY,
/* (31) Bad file number*/
SYS_FS_ERROR_BADF,
/* (32) File too large*/
SYS_FS_ERROR_FBIG,
/* (33) Invalid parameter*/
SYS_FS_ERROR_INVAL,
/* (34) No space left on device*/
SYS_FS_ERROR_NOSPC,
/* (35) No more memory available*/
SYS_FS_ERROR_NOMEM,
/* (36) No data/attr available*/
SYS_FS_ERROR_NOATTR,
/* (37) File name too long*/
SYS_FS_ERROR_NAMETOOLONG
} SYS_FS_ERROR;
1.2.7.4.53 Summary
Lists the various error cases.
1.2.7.4.53 Description
This enumeration lists the various error cases. When the application calls for a file system function which has a return type of SYS_FS_RESULT and if the return value is SYS_FS_RES_FAILURE, the application can know the specific reason for failure by calling the SYS_FS_FileError function.
The return value of SYS_FS_FileError function will be one of the enumeration of type SYS_FS_ERROR.
1.2.7.4.53 Remarks
None.