1.2.7.4.27 SYS_FS_DirRead Function

1.2.7.4.27 C

SYS_FS_RESULT SYS_FS_DirRead
(
SYS_FS_HANDLE handle,
SYS_FS_FSTAT *stat
);

1.2.7.4.27 Summary

Reads the files and directories of the specified directory.

1.2.7.4.27 Description

This function reads the files and directories specified in the open directory.

The File System supports 8.3 file name(Short File Name) and also long file name. 8.3 filenames are limited to at most eight characters, followed optionally by a filename extension consisting of a period . and at most three further characters. If the file name fits within the 8.3 limits then generally there will be no valid LFN for it.

For FAT File System:

  • If LFN is used the stat structure's altname field will contain the short file name and fname will contain the long file name. The "lfname" member of the SYS_FS_FSTAT is not applicable for FAT. It has to be initialized to NULL before calling the API. If "lfname" is not NULL, then first byte of lfname will be set to zero indicating no file found.

For other File Systems based on their implementation:

  • If LFN is used then the "lfname" member of the SYS_FS_FSTAT structure should be initialized with the address of a suitable buffer and the "lfsize" should be initialized with the size of the buffer. Once the function returns, the buffer whose address is held in "lfname" will have the file name(long file name).

  • The stat structure's fname field will contain the SFN and if there is a valid LFN entry for the file then the long file name will be copied into lfname member of the structure.

1.2.7.4.27 Precondition

A valid directory handle must be obtained before reading a directory.

1.2.7.4.27 Parameters

ParametersDescription
handleDirectory handle obtained during directory open
statPointer to SYS_FS_FSTAT, where the properties of the open directory will be populated after the SYS_FS_DirRead function returns successfully

1.2.7.4.27 Returns

SYS_FS_RES_SUCCESS - Indicates that the directory read operation was successful. End of the directory condition is indicated by setting the fname and lfname (if lfname is used) fields of the SYS_FS_FSTAT structure to '\0'.

SYS_FS_RES_FAILURE - Indicates that the directory read operation was unsuccessful. The reason for the failure can be retrieved with SYS_FS_Error or SYS_FS_FileError.

1.2.7.4.27 Example

// For FAT File System

SYS_FS_HANDLE dirHandle;
SYS_FS_FSTAT stat;

dirHandle = SYS_FS_DirOpen("/mnt/myDrive/Dir1");

if(dirHandle != SYS_FS_HANDLE_INVALID)
{
    // Directory open is successful
}

if(SYS_FS_DirRead(dirHandle, &stat) == SYS_FS_RES_FAILURE)
{
    // Directory read failed.
}
else
{
    // Directory read succeeded.
    if (stat.fname[0] == '\0')
    {
        // reached the end of the directory.
    }
    else
    {
        // continue reading the directory.
    }

}
// For other File Systems with LFN support

SYS_FS_HANDLE dirHandle;
SYS_FS_FSTAT stat;

char CACHE_ALIGN longFileName[512];

dirHandle = SYS_FS_DirOpen("/mnt/myDrive/Dir1");

if(dirHandle != SYS_FS_HANDLE_INVALID)
{
    // Directory open is successful
}

// If long file name is used, the following elements of the "stat"
// structure needs to be initialized with address of proper buffer.
stat.lfname = longFileName;
stat.lfsize = 512;

if(SYS_FS_DirRead(dirHandle, &stat) == SYS_FS_RES_FAILURE)
{
    // Directory read failed.
}
else
{
    // Directory read succeeded.
    if ((stat.lfname[0] == '\0') && (stat.fname[0] == '\0'))
    {
        // reached the end of the directory.
    }
    else
    {
        // continue reading the directory.
    }

}

1.2.7.4.27 Remarks

None.