23.7.1.1 Step 1: Configure the MSS FIC Sub-Block
As shown in the following figure, the FIC configurator (applies to both FIC_0 and FIC_1) is organized as follows. In the left panel, the following can be configured:
- The MSS to the FPGA fabric interface
- Advanced AHB-Lite options
- The FPGA fabric address regions (MSS master view) – available in FIC_0 configurator only
In the right panel, a dynamic picture displays the high level block diagram of the architecture chosen. The picture changes when any option in the MSS to FPGA fabric interface group is configured.