2.8.55 CANx_MailboxIsReady Function
C
bool CANx_MailboxIsReady(CAN_MAILBOX_NUM mailbox) // x - Instance of the CAN peripheral
Summary
Returns true if Mailbox is ready otherwise false.
Precondition
CANx_Initialize must have been called for the associated CAN instance.
Parameters
Param | Description |
---|---|
mailbox | Mailbox number |
Returns
true - Mailbox is ready and Mailbox data registers can be read/written.
false - Mailbox is not ready and Mailbox data registers can not be read/written.
Example
if (CAN0_MailboxIsReady(CAN_MAILBOX_0))
{
//Mailbox is ready and Mailbox data registers can be read/written.
}
Remarks
None.