2.3.40 ADC_EOSStatusGet Function
C
bool ADC_EOSStatusGet(ADC_CORE_NUM core)
Summary
Indicates whether End of scan interrupt flag is set on the specified ADC core
Description
Indicates whether End of scan interrupt flag is set on the specified ADC core
Precondition
ADCx_Initialize() function must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
core | ADC core n |
Returns
bool - True if EOS interrupt flag is set, False if EOS interrupt flag is not set
Example
if (ADC_EOSStatusGet(ADC_CORE_NUM1)) { // ADC conversion is complete. Read the conversion result. }
Remarks
None