2.3.30 ADC_ComparisonEventResultIsReady Function
C
bool ADC_ComparisonEventResultIsReady(void)
Summary
Returns the status of the Comparison event
Description
This function returns the status of the Comparison event whether comparison event has occurred and result is available
Precondition
ADC_Initialize() function must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
void | None |
Returns
bool - status of the comparison event false: No comparison event true: At least one comparison event has occurred
Example
bool comp_event; ADC_Initialize(); ADC_ChannelsEnable(ADC_CH0); ADC_ConversionStart(); comp_event = ADC_ComparisonEventResultIsReady(); if (comp_event) { result = ADC_ChannelResultGet(ADC_CH0); }
Remarks
None