2.3.47 ADC_GlobalInterruptsStatusGet Function

C

ADC_GLOBAL_INT ADC_GlobalInterruptsStatusGet(void)

Summary

Returns the global interrupt status

Description

This function returns the global interrupt status

Precondition

ADCx_Initialize() function must have been called first for the associated instance.

Parameters

None

Returns

ADC_GLOBAL_INT - bitwise OR of the following macros indicating global interrupt event status: ADC_GLOBAL_INT_PFFHFUL ADC_GLOBAL_INT_PFFRDY ADC_GLOBAL_INT_PFFOVF ADC_GLOBAL_INT_PFFUNF ADC_GLOBAL_INT_VREFRDY ADC_GLOBAL_INT_VREFUPD ADC_GLOBAL_INT_CRRDY1

Example

ADC_GLOBAL_INT adcGlobalIntStatus;

adcGlobalIntStatus = ADC_GlobalInterruptsStatusGet();

Remarks

None