20.2.3.2.3 Breakdown

Displays a breakdown of power usage of the currently selected block. Use the drop-down list to select whether to display the power breakdown by type of component, instance, or clock domain.

When you select By Type from the drop-down list, the Analysis tab displays a breakdown of the selected block's power usage by the following types:

  • Net
  • Gate
  • I/O
  • Memory
  • Core Static
  • Banks Static
  • Analog

Any static power used by instances of a component in a design will be included in the appropriate category. As a result, the sum of the power in breakdown by type will equal the total of the static and dynamic power consumption of the design. Percentages displayed are fractions of the total power. Global nets are included in the net power types. To obtain the power of a clock, select breakdown by clock domain.

When you select By Clock Domain from the drop-down list, the Analysis tab displays a breakdown of the power usage by the clock domain that the power is drawn from. For each clock domain, the power and percentage of power drawn are displayed. Dynamic power is accounted for in breakdown by clock, but static power is not associated by any clock.

Whether you selected By Type, By Instance or By Clock Domain, you can customize which columns are displayed in the grid by right-clicking the column headers. To exclude a column, remove its checkmark from the right-click menu. Right-click a column header to set the column default size for the selected column or for all columns, sort the values in ascending or descending order, or customize columns.

To sort the contents of a column, double-click a column header.

To export the contents of the grid to a file, from the File menu, select Export Grid or click its associated toolbar button.

To print the grid, from the File menu, select Print Grid or click its associated toolbar button. To copy the grid, from the Edit menu, select Copy Grid or click its toolbar button.

To copy the chart, click the contents of the chart, and from the right-click menu, select Copy Chart to Clipboard. To export the chart, click the contents of the chart, and from the right-click menu, select Export Chart to File.

To rotate the chart by 90 degrees, click the contents of the chart, and from the right-click menu, select Rotate Chart Clockwise or Rotate Chart Counter-Clockwise.

To view an instance properties, right-click any instance and select Instance Properties . This brings the Instance Properties window, which displays the instance name, type and power and other properties specific to each type of instance, see image below.

Figure 20-6. Instance Properties: Gate
þÿ

The Instance Properties allows you to access a list of pins of a gate and to check their domain and frequency.