21.7.5 Understanding Explicit Clocks

Explicit clocks are pins or ports connected to the clock pin of one or more sequential component, and where each clock is one of the following:
  • The output of a PLL
  • An input port that does not get gated between the source and the clock pins it drives
  • The output pin of a sequential element that does not get gated between the source and the clock pins it drives
  • Any pin or port on which a clock constraint was specified
By default, SmartTime displays domains with explicit clocks in the Timing Analysis View. You can browse these domains in the Domain Browser of the Timing Analysis View.
Figure 21-26. Explicit Clocks
þÿ