37.7.46 USB LPM Control Register
Symbol | Description | Symbol | Description | Symbol | Description |
---|---|---|---|---|---|
R | Readable bit | HC | Cleared by Hardware | (Grey cell) | Unimplemented |
W | Writable bit | HS | Set by Hardware | X | Bit is unknown at Reset |
K | Write to clear | S | Software settable bit | — | — |
Name: | LPMCNTRL |
Offset: | 0x1362 |
Reset: | 0x0000 |
Property: | PAC Write-Protection |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
LPMNAK | LPMEN[1:0] | LPMRES | LPMXMT | ||||||
Access | R/W | R/W | R/W | R/W | R/W | ||||
Reset | 0 | 0 | 0 | 0 | 0 |
Bit 4 – LPMNAK LPM-only Transaction Setting bit
Device Mode only bit. Unimplemented in Host mode.
This bit is used to place all end points in a state such that the response to all transactions other than an LPM transaction will be a NAK.
Setting this bit to '1
'will only take effect after the USB
module has been LPM suspended. In this case, the USB device will continue to NAK
until this bit has been cleared by software.
Value | Description |
---|---|
0 | Normal transaction operation |
1 | All endpoints will respond to all transactions other than an LPM transaction with a NAK |
Bits 3:2 – LPMEN[1:0] LPM Enable bits
Device Mode only bit. Unimplemented in Host mode.
Value | Description |
---|---|
11 | LPM Extended transactions are supported |
10 | LPM and Extended transactions are not supported |
01 | LPM mode is not supported but Extended transactions are supported |
00 | LPM Extended transactions are supported |
Bit 1 – LPMRES LPM Resume bit
When in Device mode:
This bit is used by software to initiate resume (remote wakeup). This bit differs from the classic RESUME bit in the POWER register (address offset 0x0001) in that the RESUME signal timing is controlled by hardware. When software writes this bit, resume signaling will be asserted for 50us. This bit is self-clearing.
1
= Initiate resume (remote wake-up). Resume signaling is
asserted for 50 µs.
0
= No resume operation
This bit is self-clearing.
When in Host mode:
This bit is used by software to initiate a RESUME from the L1 State. This bit differs from the classic RESUME bit in the POWER register (address offset 0x0001) in that the RESUME signal timing is controlled by hardware. When software writes this bit, resume signaling will be asserted for a time specified by the HIRD field in the LPMATTR register.
1
= Initiate resume
0
= No resume operation
This bit is self-clearing.
Bit 0 – LPMXMT LPM Transition to the L1 State bit
When in Device mode:
1 = USB module will transition to the L1 state upon the receipt of the next LPM
transaction. LPMEN must be set to ‘0b11
. Both LPMXMT and LPMEN
must be set in the same cycle.
0 = Maintain current state
When LPMXMT and LPMEN are set, the USB module can respond in the following ways:
- If no data is pending (all TX FIFOs are empty), the USB module will respond with an ACK. The bit will self-clear and a software interrupt will be generated.
- If data is pending (data resides in at least one TX FIFO), the USB module will respond with a NYET. In this case, the bit will not self-clear however a software interrupt will be generated.
When in Host mode:
Software should set this bit to transmit an LPM transaction.
1 = USB module will transmit an LPM transaction. This bit is self-clearing and will be immediately cleared upon receipt of any Token or three time-outs have occurred.
0 = Maintain current state