21.4.27 sd_disconnect_instance
(Ask a Question)Description
This tcl command clears all the connections on an instance in a SmartDesign component.
Note: This command is not required to build a
                SmartDesign component. This command maps to an interactive user action in the
                SmartDesign Canvas and will not be present in the exported SmartDesign component Tcl
                description.
sd_disconnect_instance -sd_name {smartdesign component name} \
                       -instance_name {instance name}Arguments
| Parameter | Type | Description | 
|---|---|---|
sd_name  | string  | Specifies the name of the SmartDesign component. It is mandatory.  | 
instance_name  | string  | Specifies the name of the instance for which all the connections must be cleared. It is mandatory.  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Parameter 'instance_name' has illegal value.  | 
None  | Required parameter 'instance_name' is missing.  | 
None  | Parameter 'sd_name' has illegal value.  | 
None  | Required parameter 'sd_name' is missing.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'sd_disconnect_instance -sd_name "sd_name" -instance_name "[instance_name]+"'.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
This example disconnects {RAM1K18_1" instance.
sd_disconnect_instance -sd_name {sd1} -instance_name {RAM1K18_1}See Also
sd_rename_instance
sd_update_instance
sd_delete_instances
sd_duplicate_instance