21.4.18 sd_create_scalar_net
(Ask a Question)Description
This Tcl command creates a scalar net in a SmartDesign component. Any net created must be connected to two or more ports/pins using the command "sd_connect_net_to_pins".
Note: This command is not required to build a SmartDesign component. It is not exported when user selects 'Export Component Description(Tcl)' on a SmartDesign component. This command is used to manually create a Tcl script and specify a new name to the net that connects two or more ports/pins.
sd_create_scalar_net -sd_name {smartdesign component name} \
                     -net_name {net name}Arguments
| Parameter | Type | Description | 
|---|---|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| net_name | string | Specifies the name of the net added to the SmartDesign component. It is mandatory. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Required parameter 'net_name' is missing. | 
| None | Required parameter 'pin_names' is missing. | 
| None | Required parameter 'sd_name' is missing. | 
| None | Unconnected input pin instance_name:pin_name | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_connect_net_to_pins -sd_name "sd_name" -net_name "net_name" -pin_names "[pin_names]+"'. | 
| None | Parameter 'net_name' has illegal value. | 
| None | Net 'net_name' does not exist. | 
| None | The component '' doesn't exist. | 
| None | The component 'component_name' doesn't exist. | 
| SDCTRL05 | Pin 'pin_or_port_name' does not exist. | 
| None | Cannot promote pin 'pin_name' on 'instance_name' to top because it is already connected to a top level port. | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following example creates a scalar net with "clk_net" name in a "Top" component and connects CLKRAM64x12_0:R_CLK, RAM64x12_0:W_CLK ports via clk_net net:
Note: This new net is visible in the UI only when it is connected to two or more ports/pins using the command sd_connect_net_to_pins shown below.
sd_create_scalar_net -sd_name {Top} -net_name {clk_net}
sd_connect_net_to_pins -sd_name {Top} -net_name {clk_net} \
                       -pin_names {CLKRAM64x12_0:R_CLK RAM64x12_0:W_CLK}See Also
- sd_create_scalar_port