21.4.30 sd_hide_bif_pins
(Ask a Question)Description
This tcl command hides one or more already exposed internal scalar or bus pins/ports of a Bus Interface pin/port.
sd_hide_bif_pins -sd_name {smartdesign component name} \
                 -bif_pin_name {name of the bif pin or port} \
                 -pin_names {pins or ports to be exposed}Arguments
| Parameter | Type | Description | 
|---|---|---|
sd_name  | string  | Specifies the name of the SmartDesign component. It is mandatory.  | 
bif_pin_name  | string  | Specifies the name of the Bus Interface pin for which the internal pins must be hidden. It is mandatory.  | 
pin_names  | string  | Specifies the bus interface internal pin/port names to be hidden. It is mandatory.  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Parameter 'pin_names' has illegal value.  | 
None  | Required parameter 'pin_names' is missing.  | 
None  | Parameter 'bif_pin_name' has illegal value.  | 
None  | Required parameter 'bif_pin_name' is missing.  | 
None  | Parameter 'sd_name' has illegal value.  | 
None  | Required parameter 'sd_name' is missing.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'sd_hide_bif_pins -sd_name "sd_name" -bif_pin_name "bif_pin_name" -pin_names "pin_names"'.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
This example hides "TX_PLL_LOCK_0" pin of "CLKS_FROM_TXPLL_0" bif pin.
sd_hide_bif_pins -sd_name {SD1} \
                 -bif_pin_name {CLKS_FROM_TXPLL_0} \
                 -pin_names{TX_PLL_LOCK_0}See Also
sd_show_bif_pins
sd_delete_bif_pin