Description
This Tcl command renames a pin group on an instance in a SmartDesign component.
sd_rename_pin_group -sd_name {smartdesign component name} \
                    -instance_name {instance name} \
                    -current_group_name {current pin group name} \
                    -new_group_name {new pin group name}
Arguments
| Parameter | Type | Description | 
|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| instance_name | string | Specifies the name of the instance on which the pin group is present. It is mandatory. | 
| current_group_name | string | Specifies the name of the pin group to be renamed. It is mandatory. | 
| new_group_name | string | Specifies the new name of the pin group. It is mandatory. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'sd_name' is missing. | 
| None | Required parameter 'instance_name' is missing. | 
| None | Required parameter 'current_group_name' is missing. | 
| None | Required parameter 'new_group_name' is missing. | 
| None | Parameter 'param' is not defined. Valid command formatting is 'sd_rename_pin_group -sd_name "sd_name" -current_group_name "current_group_name" -new_group_name "new_group_name" -instance_name "instance_name"'. | 
| SDCTRL05 | Pin 'MyGroup' does not exist. | 
| None | Parameter 'current_group_name' has illegal value. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
This command renames "Group" to "MyNewGroup" on the "COREAXINTERCONNECT_C0_0" instance in the "TOP" design:
sd_rename_pin_group -sd_name {TOP} \
                    -instance_name {COREAXINTERCONNECT_C0_0} \
                    -current_group_name {Group} \
                    -new_group_name {MyNewGroup}
See Also
- sd_create_pin_group
 - sd_add_pins_to_group