21.4.15 sd_create_bus_port
(Ask a Question)Description
This tcl command creates a bus port of a given range in a SmartDesign component.
sd_create_bus_port -sd_name {smartdesign component name} \
                   -port_name {port name} \
                   -port_direction {IN|OUT|INOUT} \
                   -port_range {[left range index:right range index]}Arguments
| Parameter | Type | Description | 
|---|---|---|
sd_name  | string  | Specifies the name of the SmartDesign component. It is mandatory.  | 
port_name  | string  | Specifies the name of the bus port added to be SmartDesign component. It is mandatory.  | 
port_direction  | string  | Specifies the direction of the bus port added to the SmartDesign component. It is mandatory.  | 
port_range  | string  | Specifies the range of the bus port added to the SmartDesign component. The range is defined by the left and rightindices. It is mandatory. The range must be specified inside the square brackets.  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Parameter 'port_range' has illegal value.  | 
| None | Required parameter 'port_range' is missing.  | 
| None | Parameter 'port_direction' has illegal value.  | 
| None | Required parameter 'port_direction' is missing.  | 
| None | Parameter 'port_name' has illegal value.  | 
| None | Required parameter 'port_name' is missing.  | 
| None | Parameter 'sd_name' has illegal value.  | 
| None | Required parameter 'sd_name' is missing.  | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_create_bus_port -sd_name "sd_name" -port_name "port_name" -port_direction "IN | OUT | INOUT" -port_range "port_range"'.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
This example creates bus port with name "test_port13", direction "OUT" and in [9:36] range.
sd_create_bus_port -sd_name {top} \
                   -port_name {test_port13} \
                   -port_direction {OUT} \
                   -port_range {[9:36]}sd_create_bus_port -sd_name {top} \
                   -port_name {test_port4} \
                   -port_direction {IN} \
                   -port_range {[31:0]}See Also
sd_create_bus_net